AnsweredAssumed Answered

Limiting frequency of Local Oscillator

Question asked by ashish.30 on Dec 22, 2015
Latest reply on Jan 7, 2016 by LKelly

Hi,

 

I am working on an IQ Modulator/Demodulator based control system. My frequency of operation is 2860 MHz, so I wish to purchase ADRF6720-EVALZ and ADL5380-EVALZ for the testing purpose. But from the manual of ADRF6720, I could see that internal LO gives a facility to generate LO signal upto 2855MHz and it doesn't say anything about the external LO connection ranges. I want to have a LO signal with 2860 MHz which I can provide with external generator. So, is it possible to get ADRF6720-EVALZ working with 2860MHz as it goes upto 3GHz of RF frequency output.

Outcomes