AnsweredAssumed Answered

ADP7102 ADIsimPower input capacitor error

Question asked by K1MGY on Dec 16, 2015
Latest reply on Dec 16, 2015 by K1MGY

ADIsimPower is a very nice tool.. a real time saver.  However I noticed an error in the tool for the ADP2102.

 

Using parameters for input voltage of +12V the tool specified an input capacitor rated at 6.3V.  Either that, or C1 and C2 in the diagram below are incorrectly labeled (reversed).  Easy fix on this end, but might sink young players.

 

12-16-2015 10-43-37.png

Outcomes