AnsweredAssumed Answered

AD9361

Question asked by amboyle on Dec 9, 2015
Latest reply on Dec 16, 2015 by amboyle

Block_Diagram.png

    Some initial questions to be asked the FAE:

 

  • Is it possible to measure phase shift between Tx and Rx frequency?
  • Is it possible to set the Rx center frequency to be different then the Tx frequency so the output will be an AC IF frequency, sampling this two signals will give the phase and amplitude difference. The concept block diagram is as follows:

 

  

 

  • Is it possible to change the frequency for our application from 1 to 6 Ghz without changing the hardware?
  • What is the dynamic range that can be measured in frequencies running from 1 to 6 Ghz  and for If BW of 200KHz?
  • How much time it will take to set a one frequency and perform one measurement with the DAC?

Outcomes