AnsweredAssumed Answered

Can AD9984A support 1366x768 and 1680x1050?

Question asked by SHIGETO on Dec 8, 2015
Latest reply on Dec 11, 2015 by GuenterL

I would like to convert from analog RGB to DVI.

 

Can AD9984A convert following resolution, like Nonstandard CP PLL Modes of ADV7800?

 

1280x800 @83.5MHz (Pixel Clock)

1366x768 @85.75MHz

1440x900 @106.5MHz

1600x900 @108MHz

1680x1050 @147.14MHz

1920x1080 @138.5MHz

1920x1200 @ 152MHz

 

These resolution are less than 150 MHz of pixel clock.

 

Best regards.

Outcomes