AnsweredAssumed Answered

Using TMP36 with AD8362 at 1 MHz

Question asked by Ernie on Dec 8, 2015
Latest reply on Dec 9, 2015 by enash

I have a design that is using the TMP36 to compensate for temperature changes of the AD8362 Log Amp. The input to the AD8362 is 1 MHz. The chart in the application note only goes down to 900 MHz when selecting the resisters shown in the application. How do I calculate the resistors for 1 MHz operation of this log amp?

Outcomes