AnsweredAssumed Answered

HMC772

Question asked by ADIguy on Dec 8, 2015
Latest reply on Dec 8, 2015 by bkamak

Hi,

 

I have a few questions regarding the HMC772LC4:

 

 

1. Can I use electrically and thermallyconductive epoxy like Epotek H20E to mount the device to an LTCC module instead of soldering it?

 

 

2. Will the device work with a +3.3 V supply, and are there any issues with using the HMC772LC4 with Vdd = 3.3 V?

 

 

3. If I use multiple HMC772LC4 in a circuit, will I need to supply a separately adjustable Vgg gate bias voltages to each device?

 

Thanks.

Outcomes