AnsweredAssumed Answered

SigmaStudio for SHARC prompt of Compatibility

Question asked by Stephan.wu on Dec 8, 2015
Latest reply on Dec 23, 2015 by DaveThib

Hello,

One of my customers has got a problem with SigmaStudio for SHARC. A prompt of version compatibility comes when a project is opened.

The DSP is ADSP-21489. SigmaStudio version is 3.11. SigmaStudio for SHARC version is 2.2.0. SHARC Audio Toolbox version is 2.0.0. Operating system is Windows 7 32-Bit.

Prompt is as blow,

Could you please give some suggestions?

Thanks a lot!

 

Compiler###### IC 1 ######

 

SigmaStudio for SHARC Plug-Ins used in Schematic under IC 1
[Module Name : Created with : Loaded with]

 

  1. 1. Off chip Delay( External Port) : 2.0.0 : 2.0.0
    2. Off chip Delay( External Port)50ms : 1.0.0 : 1.0.0
    3. Off chip Delay( External Port)20ms : 1.0.0 : 1.0.0
    4. Off chip Delay( External Port)250ms : 1.0.0 : 1.0.0
    5. Off chip Delay( External Port)80ms : 1.0.0 : 1.0.0
    6. Off chip Delay( External Port)500ms : 1.0.0 : 1.0.0

 

* indicates that the version compatibility check has been skipped/failed for the Plug-In.
In such cases, the Schematic may be corrupted and may not function as expected.
This can even lead to target crash when it is downloaded.
Removing failed/skipped Plug-Ins from the Schematic and re-inserting available versions of such Plug-Ins will fix the Schematic.

Outcomes