AnsweredAssumed Answered

Using the ADAU1772 at 96 kHz

Question asked by percy on Dec 7, 2015
Latest reply on Dec 7, 2015 by DaveThib

I have the ADAU1772 configured for 48 kHz. I now need to use it at 96 kHz.

I have the MCLK at 10 MHz and the PLL out is 1024 x 48 kHz = 49.152 MHz.

So can someone tell me what changes I need to make to get 96 kHz.

The code I am using is sample code from a project that uses the part on the Zedboard

Thanks

Outcomes