AnsweredAssumed Answered

on the AD633, can V- be connected to GND?

Question asked by Belenie on Dec 4, 2015
Latest reply on Dec 10, 2015 by Belenie

Hello,

 

My customer has the following question:

 

if I am using the AD633 to multiply two signals that are between 0V to positive 10V only (single quadrant operation) do I need a negative voltage on V- or can I connect V- to ground?

 


Thanks,

Belenie

Outcomes