AnsweredAssumed Answered

ADV7513 - Queries on HPD Input

Question asked by elvin.joy@ittiam.com on Dec 3, 2015
Latest reply on Dec 3, 2015 by GuenterL

Hi,

 

I have the following queries regarding ADV7513 HPD (Hot Plug Detect) input.

 

1. Is HPD input edge triggered or level triggered?

 

2. If it is level triggered, what is the duration for which the HPD should be asserted to indicate the connection to the sink?

 

3. If it is edge triggered, can a spike of voltage greater that 1.3V (minimum high level input voltage for HPD) cause the HPD to be asserted?

 

Regards,

Elvin

Outcomes