AnsweredAssumed Answered

ADL5380 IP3 and output voltage swing

Question asked by nik on Jun 14, 2011
Latest reply on Jun 15, 2011 by Qui

Greetings,

 

The specification for the ADL5380 states that the input P1dB is +11.6 dBm, conversion gain is +6.9 dB and output voltage swing is +2 Vp-p.

 

The note at the top of the spec table states that that test conditions is with a load of  450 Ohms. A 2 Vp-p swing is  consistent with an output  level of +0.45 dBm.   But this seems inconsistent with a maximum output level before saturation of 10.6+6.9=  +17.5 dBm.  Note: I backed off 1 dB from the input P1dB.

 

Put another way can anyone tell me what the the maximum output voltage swing would be for an input of +10.6 dBm.

 

PS.  Can someone post the s2p file for the ADL5380?

 

Thank you in advance!

Outcomes