AnsweredAssumed Answered

ADN4612 and ADN2915- Schematics & supported features

Question asked by FreddyS on Nov 29, 2015
Latest reply on Nov 30, 2015 by jmarshma

Hello

I will need the schematics for the ADN4612 and ADN2915 as provided off line in

http://ez.analog.com/message/116339

 

In addition, regarding the crosspoint switch ADN4612:

   

supports limiting mode?
supports linear mode?
Is there eye monitoring?
loopback mode per port?
P/N swapping is supported--- YES
Need to support jitter at optical output (20k-80MHz) <0.3UI, (4MHz-80MHz)<0.1UI
Need data related to crosstalk inside the package
Need jitter frequency spectrum test results

 

 

Thanks

Freddy

Outcomes