AnsweredAssumed Answered

AD9963 CLKN Bypass Component Values

Question asked by rwyost on Jun 14, 2011
Latest reply on Dec 21, 2017 by Biao.H

In the datasheet for the AD9963, located in the "Driving the clock input" section on p.46, it is recommended that a 0.1µF capacitor and 39k resistor be placed in parallel on the CLKN pin when driving the CLKP pin with a 1.8V CMOS single-ended clock input.  When using a 3.3V CMOS-driven single-ended clock input, do these recommended values change?

 

Rob Yost

Outcomes