AnsweredAssumed Answered

PEYEN bit in MODE1 is causing issue

Question asked by jsksra1 on Nov 27, 2015
Latest reply on Dec 1, 2015 by jsksra1

Hi ,

 

From the datasheet of ADSP-21489, I got to know that SIMD has two processing elements, and in my program SIMD is enabled.

 

But in MODE1 register PEYEN bit is '0'. I thought to enable this by setting this bit to '1' , so that simd is enabled always, but if I do that my program is hanging in case of fileops.

 

Is it a correct way to use that bit?\

 

And if simd based dsp functions is used, then this bit will be set automatically and de-asserted back ??

 

Regards
Sravan

Outcomes