AnsweredAssumed Answered

ADP1048 - PMBus to SPI Bridge

Question asked by chr1987 on Nov 26, 2015
Latest reply on Dec 1, 2015 by chr1987

Dear all,

 

i have the Problem, that i have to connect the ADP1048 to a µC without an I²C Interface. The only available Interface is a SPI Bus. So i decided to use a I²C to SPI Bridge. The question is: The I²C to SPI Bridge can`t handle the PMBus timeout of 35ms. Could i get a Problem due to this?

 

Thank you very much!

Outcomes