AnsweredAssumed Answered

ADAU1452 ASRC

Question asked by keddy on Nov 26, 2015
Latest reply on Nov 30, 2015 by DaveThib

Hi,

 

I would like to use ADAU1452 to handle SRC of the inputs connected to serial input channel 0,1,16,17,32,33,40 and 41. Can you advise on the correct way to use the ASRC to SRC the input from 44.1kHz to 48kHz, and then output to SD1 as a 8ch I2S output? I would also like to know whether it is possible to switch the SRC dynamically through I2C control if the input can come in 44.1kHz, 48kHz, 96kHz or 192kHz?


Thanks for the advise!


Keddy Yang

Outcomes