AnsweredAssumed Answered

pcb or datasheet for HMC767LP6CE

Question asked by tiapassu on Nov 23, 2015
Latest reply on Nov 27, 2015 by dyoung1

Greetings to all, I have previously tested and burned the FB4 component on of the HMC767LP6CE device. Noting the difference between PCB and datasheet (on the pcb where there is 15V for the tuning voltage and 5.5V for the VCO voltage while 13V and 5.25V max as VCO on the datasheet), I wanted to know to which maximum threshold I have to limit myself, to avoid the burnt of the device if there is some  electronics below that brings the voltage to that value. Can someone help me with this problem?

Outcomes