AnsweredAssumed Answered

About reference for  AD7176-2

Question asked by Tarzan on Nov 20, 2015
Latest reply on Dec 4, 2015 by Tarzan

Hi there,

 

I have questions about AD7176-2.

According to the datasheet, there are some recommended external reference like ADR441.

#1,Do you think it's fine to use one piece of ADR441 for two or three pieces of AD7176-2?

#2,About the current load of reference pin,

   Is it okay to consider that thee spec of " Average Reference Input Current" is equal to the load current?

#3,Average Reference Input Current is ±72 μA/V , so If it's used as 2.5V, the load current is 2.5V*±72 μA/V?

#4,The datasheet says it requres 4.7uF capacitors for refpin, I'm worried about the stability of ADR441.

   Do you know how much the cap is the maximum for ADR441?

 

Best regards,

Tarzan

Outcomes