AnsweredAssumed Answered

max input voltage to ad8138

Question asked by tweekzilla on Nov 18, 2015
Latest reply on Nov 19, 2015 by KRZ

Is there a max input voltage above the rail voltage that the ad8138 can see before damage?  The opamp before the driver operates at a +-5V rail (rail-to-rail), however, for power reasons the adc driver operates at +-4V.  Would damage occur if +5V was presented on the +IN terminal on the device?

Outcomes