AnsweredAssumed Answered

Frequency stepping with ADF4158

Question asked by rajasrijan on Nov 18, 2015
Latest reply on Aug 1, 2016 by rbrennan

HI all,

 

I'm working on Stepped frequency continuous wave radar where I need to generate frequencies from 500MHz to 3GHz in steps 2.5MHz. I see from Documents of ADF4158 that it is able to output ramp. Will it be possible to step through frequencies, with ADF4158, in increments of 2.5MHZ? Is there a better way to do this than using VCO-PLL combo (perhaps DDS or only VCO), keeping in mind that later I would like to switch to 0.5GHz to >6GHz by switching as little component as possible? 0.5Ghz - 3GHz is for prototype.

 

thanks

Outcomes