AnsweredAssumed Answered

ADV7125BCPZ170

Question asked by cli@dit on Jun 10, 2011
Latest reply on Jun 14, 2011 by Sybren

Hi,

 

I need a RGB to VGA IC. There are two I am interested in, ADV7125BCPZ170 and ADV7125JSTZ240. When I requested sample for both of them, it indicateded that ADV7125BCPZ170 is 5V only. Since ADV7125BCPZ170 has different package than other ADV7125, I would like to get the clarification if ADV7125BCPZ170 is +5V only. If this is the case, can ADV7125BCPZ170 interface directly with +3.3V RGB sources? Thank you.

 

Best Regards,

 

Chunte Li

Outcomes