AnsweredAssumed Answered

AD7367-5 circuit diagrams

Question asked by silence_stone on Nov 14, 2015
Latest reply on Nov 17, 2015 by silence_stone

When I used the AD7367-5 for a single-end  bipolar range-±5V analogue input signal,I couldn't 100% be sure that could that chip work in the single-ended model,since  Figure 21 about typical connection diagram in the data sheet AD7367 has some conflict with Fifure 1 in the reference  design CN0042 about the analog input signal range.Considering about I couldn't get the right output and   the AD7367-5  data sheet has some mistake that makes me couldn't trust it,can someone solve my donbt,or tell me is the circuit diagrams in the attachment correct or not ? Thanks a lot无标题.png

Outcomes