AnsweredAssumed Answered

ADP5037 VOUT1 output fails to start (sometimes)

Question asked by JeffP on Nov 12, 2015
Latest reply on Dec 4, 2015 by JeffP

I'm using an ADP5037 to generate 4 supply rails in a sequenced-startup configuration.  Sometimes the VOUT1 converter fails to turn on as expected.  It appears to be related to the ramp time on my input power--if I use a power supply with a faster ramp time (<5 ms) I seem to get reliable startup.

 

Here's my configuration:

AVIN=VIN1=VIN2 = 3.3V

VOUT1 set for 2.5V

VOUT2 set for 1.3V

VOUT3 set for 3.0V

VOUT4 set for 1.3V

 

The startup sequence is:

EN2 and EN4 (tied together) are asserted and the corresponding output voltages appear.

EN1 is asserted ~0.6ms later but VOUT1 sometimes turns on and sometimes does not.

EN3 is not asserted during power up.

 

Plots showing turn turn on and failed turn-on sequence are attached.

 

I've noticed that toggling EN1 will cause VOUT1 to start.

 

Any thoughts as to why VOUT1 won't turn on initially during some power-up sequences?

 

Thanks

Outcomes