AnsweredAssumed Answered

HSC - ADC - EVALC Capture Board with AD9633. Communication with C code or Labview application.

Question asked by lbh on Nov 10, 2015
Latest reply on Nov 20, 2015 by DougI

Hello,

 

I have acquired the HSC-ADC- EVALC capture board to interfacing and capture data from the ADC AD9633 evaluation board. I don't have problems using the provided software, VisualAnalog. I can capture the data from the ADC without any issues.

 

However, I need to build an application (Labview or C) able to capture the data from the board in automatic version, without the VisualAnalog limitations. My question is, there are some way to achieve this objective?

 

I have read that there are drivers that enable interfacing the HSC-ADC-EVALCZ. These are the following dlls:

 

     - HadboardApi.dll

     - HadSdpSupport.dll

     - sdpApi1.dll

 

Can I use these dll in a C code or in a Labview application to capture the data from the baords? If the answer is affirmative, there are examples that help me to use these dlls? Unfortunately, I don't know that I have to do with the methods and properties that these dlls provide.

 

Any help or guide for me are appreciated.

 

Sorry for my english and thank you for your attention.

Outcomes