AnsweredAssumed Answered

ADV7181 CP 8bit mode

Question asked by rinivanzetten on Nov 10, 2015
Latest reply on Nov 12, 2015 by GuenterL

We use the ADV7181-D connected to freescale IMX-6 (using a Vairiscite SOM-SOLO module).

When in SD (CVBS) mode this works fine. output of the ADV7181 is 8Bits BT565 mode.

We also want to use the CP (VGA) mode but this gives some problems.

Can the ADV7181 in CP mode output data in 8 BITS (SDR) ?

if yes,  Can it enable the BT565 mode ?

 

If not, is there an alternative chip (eg ADV7842) which can output 8 bit (SDR) in VGA mode ?

 

Regards,

 

Rini

Outcomes