AnsweredAssumed Answered

AD9249 input voltage range

Question asked by ishino@fujiele.co.jp on Nov 5, 2015
Latest reply on Nov 9, 2015 by DougI

Hello ADI team.

I have a question.  Currently, the are our adopt AD9249 / 9681 in a single-ended

In use, the input voltage from the input range (0.4V ~ 1.4V) is barely

When raised, the greater the number clock, that of a digital noise is.

Because my customer is forced using the product of the differential input recommended in the single-ended input, Although it is well aware that self-responsibility for this matter

I want the thing if you have any information.

Outcomes