AnsweredAssumed Answered

looking for a ad8302 type devices for temp range upto +125c

Question asked by engineersForge on May 31, 2011
Latest reply on Aug 1, 2011 by engineersForge

hello,

 

i require a device like the ad8302 gain and phase comparator.

 

basically i need to compare two sine waves in the range of 100mVpp to 2Vpp in two frequencies, 400KHz and 2MHz. i need to find the phase difference and amplitude difference between them. phase difference will be from 0 to 100 degrees, and amplitude difference will be from 0V to 500mV. And the device needs to be high temp (+125C).

 

if there is other combination of ics to do this that would also work, since i will be using a microcontroller to analyze the data, so pwm, adc... methods as outputs will work.

 

any info is much appreciated.

Outcomes