AnsweredAssumed Answered

Code size and the Boot Problem

Question asked by hotkernel on May 30, 2011
Latest reply on Jul 2, 2011 by hotkernel

Hi All,

I'm using the BF512F which boots from internal SPI flash.The internal flash's size is 512K bytes.

If I use the emulator and load the dxe file,the program can run well.But when I create the
ldr file with a correct init.dxe and download it(The ldr file size is 295K bytes) to the internal flash,the board can't boot well.If I comment any code to make the ldr file size smaller than 285K bytes.The smaller ldr file in the flash can boot well.It seems that the code size can't bigger than 285K bytes. Could any one tell me why,thanks!

Outcomes