AnsweredAssumed Answered

Internal Flash RunTime programming

Question asked by AviMagos on May 12, 2011
Latest reply on May 13, 2011 by AviMagos

Hi,

 

I'm working with BF516F/BF518F with internal flash.

 

I want to implement run-time flash programming i.e. a flash driver that can be called by the software running from the DRAM and allows it to read/write the internal flash directly. (for purposes of software update on-the-go etc).

 

The only flash driver examples I've seen are to be compiled seperately and burned to a special reserved section in the flash for use with JTAG when uploading software from PC.

 

Is there any example for such a -runtime driver?

Is there any documentation of the flash memory-map (which addresses are reserved for boot loader/ flash driver etc?)?

 

Thanks,

Avi & Amit.

Outcomes