AnsweredAssumed Answered

Windows7 x64 + Matlab-Simulink-x64 + VDSP++ + Sharc

Question asked by bookevg on May 11, 2011
Latest reply on May 12, 2011 by ColinJ

I has the model of my control system and control object in Simulink.

But when I wanted to transfer my control system to VDSP++ then I run command <adivdspsetup> in Command Window then I had next error:

??? Error using ==> adivdspsetup at 14
You cannot invoke ADIVDSP on a 64-Bit Microsoft(R) Windows(R) platform.
The IDE Link adaptor for use with Analog Devices(TM) VisualDSP++(R) is not supported on this
platform.
Refer to the IDE Link System Requirements for platforms supported by this adaptor.

 

In file adivdspsetup.m:

%% Check if this platform is supported
linkfoundation.autointerface.baselink.checkPlatformSupport('adivdsp', ...
adivdspext.Utilities.getPlatformsSupported());

 

Would you do to work VDSP++ with Matlab-Simulink-x64?

 

This text is wrong:

You cannot invoke ADIVDSP on a 64-Bit Microsoft(R) Windows(R) platform.

 

If I used Matlab-Simulink-x86 in  Windows7 x64 it would be ok.

Outcomes