AnsweredAssumed Answered

Low output power level of HMC832 Evaluation Kit

Question asked by AkiraO on Oct 29, 2015
Latest reply on Oct 29, 2015 by DonY

Hello,

 

Could you please support us?

My customer using HMC832 Evaluation Kit and he has a trouble about output power level. When he set output frequency around 2210MHz, output power level is -29.7dBm. And also 2211MHz is -24.5dBm and 2204MHz is -18.9dBm. On the other hand, 1092MHz is -0.85dBm, 2170MHz is -2.66dBm and 2230MHz is -5.87dBm.

 

The customer using "lmc832_fracfb_Low_I.txt", which is include Evaluation Kit, and just changed OUT Freq Desired on the GUI.

 

Is the cause of this probrem from hard ware or resister setting?

 

Best regards,

Akira

Outcomes