AnsweredAssumed Answered

Connections between AD8338 and AD9226

Question asked by FiveSheep on Oct 29, 2015
Latest reply on Sep 19, 2017 by PMH

AD8338 has an internal VREF at 1.5V,we want to set the output common-mode votage to 2.0V by adding resistors from summing nodes to COMM,so that AD9226,the ADC,which has a VREF that has been set to 2.0V,could be directly connected with AD8338 differentially.Could this way possibly work ?

P.S. The whole system is supplied by single power.

Outcomes