AnsweredAssumed Answered

From the ADL 5566 Datasheet, i see that there are two outputs VON1 and VOP1 for  amplifier 1. If this is a differential  amplifier, what are the outputs at VON1 and VOP1 in terms of input. How do i get an output which is the difference between the two inp

Question asked by prapti on Oct 20, 2015
Latest reply on Oct 23, 2015 by JinoL

From the ADL 5566 Datasheet, i see that there are two outputs VON1 and VOP1 for  amplifier 1. If this is a differential  amplifier, what are the outputs at VON1 and VOP1 in terms of input. How do i get an output which is the difference between the two input voltages. Also, i see a small  bubble at the top of the first op-amp. What is the significance of that bubble?

Outcomes