AnsweredAssumed Answered

Exclude part of library to compile saving memory

Question asked by Joho Employee on Oct 19, 2015
Latest reply on Oct 20, 2015 by Joho

Related to: ADSP-BF592, VDSP++5.1.2

 

Using a default LDF file. As the code size grows large, I checked the memory map. I see that there is more than 1 kByte occupied by the library routines

Cplbhdr

Cplbinit

Cplbmgr

These are linked from the library file libevent532y.dlb. My application does not use cache, the scratchpad memory is used for heap and stack. My understanding is that these routines would be needed only if I would use cache.

If this is the case, how can I get rid of these as I am not using cache?

Outcomes