AnsweredAssumed Answered

The solution for over-range input of AD2S1200

Question asked by Kaos on Oct 19, 2015
Latest reply on Nov 5, 2015 by jcolao

Dear Sir/Madam,

 

I just got the following question from our customer.

 

As for your resolver AD2S1200,


What is your solution for over-range input signal like as 9.9Vp-p come from the external transformer?

Simply should we put the divided resister eg;10kohm/10kohm=1/2 scaled?

Or should we put the transformer eq;2:1=1/2 scaled at the front of sin/cos pin?


Here is updated info from cusotmer.

Customer cannot put the additional transformer on the front of AD2S1200 SIN/COS pin I heard.

And he has requested to add the resister divider circuit on there.

Do you have any solution way about this?


Thanks Kaos

Outcomes