AnsweredAssumed Answered

Synchronization signals for ADV7120 & ADV7125

Question asked by mohnishb11 on Oct 17, 2015
Latest reply on Oct 19, 2015 by GuenterL

Hi all,

I want to develop one VGA interface.

 

My input is 24-bit parallel RGB data, HSYNC & VSYNC.

My output is VGA (Analog RGB data, HSYNC & VSYNC) on a standard DE-15 VGA connector.

 

My question is:

If I use any of the 2 encoders (ADV7120 or ADV7125) to convert the digital RGB inputs to analog RGB outputs,

will there be any problem if I do not provide the sync signals (HSYNC & VSYNC) to any of these encoders & directly

pass the sync signals (HSYNC & VSYNC) to the VGA connector ??

 

Will such a system work??

Outcomes