AnsweredAssumed Answered

Export System Filesissue

Question asked by BobWalker on May 2, 2011
Latest reply on May 4, 2011 by BobWalker

When exporting System Files, the program data in the <project>_IC1.h file is 2 bytes shorter than that of the TxBuffer_IC1.dat file

 

/* DSP Program Data */
#define PROGRAM_SIZE 290
#define PROGRAM_ADDR 2048
ADI_REG_TYPE Program_Data[PROGRAM_SIZE] = {

 

NumBytes.dat:

.......

3,
4,
292,  <---------
46,
3,
3,

.........

 

There are 2 extra bytes of 0x00, 0x00 in TxBuffer_IC1.dat. I'm not sure if this will cause a problem, however I thought I'd report it anyway.

 

My function that uses data from TxBuffer.dat and NumBytes.dat is failing, whereas the default_download() function works.

I am memory limited here - default_download() is 600 bytes vs. 98 bytes for my function.

Outcomes