AnsweredAssumed Answered

ADN4600ACPZ powr supply design

Question asked by wasim_28 on Oct 9, 2015
Latest reply on Oct 16, 2015 by jmarshma

Hi,

 

I am using ADN4600 in my design . Inputs are AC-Coupled from FPGA(Kintex-7) GTX Bank and Outputs are AC-Coupled to a 2m cable via connector .

Can I use 3.3V for all the supply rails required for the IC (VCC , DVCC , VTTI , VTTO ) or I have to strictly follow the Data sheet(Rev-B Page-14 , Table 5 ) recommendation  for  Low VTTI, AC-Coupled Input  :  VCC (V) =1.8 V and VTTI (V)=1.6 .

 

Please provide the maximum power consumption details for all 8Channel in operating mode .

Outcomes