AnsweredAssumed Answered

FMCDAQ2 eval board on KCU105 fpga board - tcl script error

Question asked by ic70 on Oct 7, 2015
Latest reply on Oct 7, 2015 by ic70

I have the FMCDAQ2 eval board and the KCU105 fpga board (sold together as a kit by Avnet) that I'm trying to use to eval the adc & dac.

I downloaded the HDL source (hdl_2015_r1) as a zip file.

I also installed Vivado 2014.4.1, as required.

 

However, when I run the hdl-master/projects/daq2/kcu105/system_project.tcl script in Vivado 2014.4.1, it stops with the following error:

ERROR: [BD 5-216] VLNV <analog.com:user:util_adcfifo:1.0> is not supported for this version of the tools.

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

    while executing

"create_bd_cell -type ip -vlnv analog.com:user:util_adcfifo:1.0 util_adcfifo"

    (procedure "p_sys_dmafifo" line 26)

    invoked from within

"p_sys_dmafifo [current_bd_instance .] axi_ad9680_fifo 128 16"

    (file "system_bd.tcl" line 5)

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 97)

    invoked from within

"adi_project_create daq2_kcu105"

    (file "system_project.tcl" line 8)

 

 

What should I do?

Thanks!

- Ian

Outcomes