AnsweredAssumed Answered

AD9910 eval boards on Windows7 load setup error

Question asked by RobT on Oct 7, 2015
Latest reply on Oct 27, 2015 by JLKeip

I am running four AD9910 evaluation boards from a USB hub using the latest version of the evaluation software (setup2.0.0.0) on a Win7 computer.

Each of the 4 boards can all be accessed individually from the software without problem.

The problem I have is that after I have saved or loaded the setup, when I next select another board from 'select eval board', an error occurs: "Firmware file path is invalid! in procedure IFirmwareDownloader_DownloadFirmware of Class Module ADIClkEvalInitializerDL".

I am unable to control the board from then on.

Is there anything I can do about this?

Outcomes