AnsweredAssumed Answered

ADV7511 color problem

Question asked by d.s.e on Oct 7, 2015
Latest reply on Oct 14, 2015 by d.s.e

I have some problems getting the colors right.

 

The video input comes from a Sony FCB-EH3150 camera in 480p, 60Hz, YCbCr 4:2:2, the monitor is connected to the evaluation board via DVI. CSC is enabled.

Playing around with all the different camera and ADV7511 settings didn't produce a proper result.

Especially settings the CSC coefficients seems to have no effect.

 

Any hints?

 

 

Attached are screenshots showing the faulty image compared to an older screenshot using another camera.

Attachments

Outcomes