AnsweredAssumed Answered

ADA4960-1 work for differential input to single-ended output?

Question asked by erivard on Oct 5, 2015
Latest reply on Oct 18, 2015 by richardcer

Hi,

 

I need to convert a base-band differential input to a single-ended output, bandwidth of 4 GHz. ADA4960-1 is a fully differential amplifier, so I assume I can terminate one of the differential outputs to create a differential input to single-output buffer amplifier, but the datasheet only shows the opposite case: single ended input to differential output. Will I be able to use this part for differential in to single out? If not, is there another part that would work?

 

Thank you,

Erin

Outcomes