AnsweredAssumed Answered

Regarding Absolute Maximum rating for ADV3228

Question asked by Gautam on Oct 5, 2015
Latest reply on Oct 16, 2015 by AnnaFeB

hi

I have doubt regarding the maximum potential difference between DVCC and AVEE. As in Datasheet it is given 6V and in user manual it is shown that it takes AVCC=+5V, AVEE= -5V & DVCC = +5V. As per user mannual the maximum potential difference between DVCC and AVEE is 10V which contradict with the Datasheet. can anyone please clarify this.

 

From datasheet absolute maximum rating

1.  AVCC - AVEE <= 11V

2.  AVCC - DVCC <= 0.5V

3.  AGND - DGND <= 0.5V

then How DVCC - AVEE <= 6V.

 

 

regards

Gautam

Outcomes