AnsweredAssumed Answered

About the bandwidth supported by AD9361

Question asked by manideep on Oct 5, 2015
Latest reply on Oct 9, 2015 by info@wesbrodsky-wireless.com

hello,

 

     The maximum supported bandwidth of RX analog filter and TX analog filter are around 110 MHz and 100 MHz respectively. The above figures are calculated as per formulas given in the datasheet, here we took the maximum BBPLL frequency is 1400 MHz and divider value is 1. But the maximum bandwidth is 31 MHz as per the register settings and datasheet. We need to operate the maximum bandwidth of 60 MHz in our application, so let us know what is the maximum bandwidth supported by the AD9361.

 

     The calculation of supported sample rate from the baseband PLL frequency or let us know the divider range used in calculation of sample rate.

 

Regards,

Lakshmi.


Outcomes