AnsweredAssumed Answered

For junction temperature rating value of ADM3251E

Question asked by Laliberte on Oct 1, 2015
Latest reply on Oct 5, 2015 by RAnslow

Hi, All.

 

I’m considering the ADM3251E.

When calculated from the Operating Temperature Range Max,

Tj = Power(145mA×5.5V) × Theata_ja(47.05℃/W) + 85℃
   = 122.5℃

Would the rated value of Tj be about 150 ℃?
If there is a guaranteed value, please let me know.

 

Best Regards,

Laliberte

Outcomes