AnsweredAssumed Answered

adv7511 current consumption in standby

Question asked by quintile on Sep 29, 2015
Latest reply on Oct 13, 2015 by GuenterL

Hi,

 

I am looking for realistic figures for the power consumption of an adv7511 in standby mode.

By this I mean, with everything but hotplug detect and CEC disabled.

 

I would also like a value for the power consumption when shutdown - i.e. everything is shutdown

except the I2c interfaces, which would be used to restart the device.

 

The manual mentions values of 20mA and 300uA - Are these correct? If so how do I achieve the lower

figure, the best I have managed has been about 7mA split between the two PSU rails.

 

Many thanks for any help,

 

-Steve

Outcomes