AnsweredAssumed Answered

Error in LO frequency of ADRF6655

Question asked by ricard.castella on Sep 29, 2015
Latest reply on Oct 16, 2015 by mthahira

Hi everybody,

 

First of all let me introduce myself, my name is Ricard and I'm student of last year of telecoms degree and I want to use ADRF6655 for downconverting application. I've bought the ADRF6655-evalz board for testing but doesn't have the desired behaviour because if I set the LO frequency at 1940MHz using analog software in the output I can check that the signal generated by the LO is approximately ~22MHz more and is not fixed. Any idea?

 

Thanks for your attention.

Outcomes