AnsweredAssumed Answered

Regulator with positive input and negative output

Question asked by oscargomezf on Sep 28, 2015
Latest reply on Jan 20, 2016 by oscargomezf

Hi,

I'm trying to find out the best option for a regulator with positive input and negative output.

I need to feed six operational amplifiers with V+=(max: 12V min: 7V) and V-=-(max: 12V min: -7V) and I only have a power supply of 12V@1A.


On the whole, the total power consumption is around 600mWatts.

I don't mind to use a dual-output (+12V..+7V and -12V..-7V), but I would like to make sure to choose the best option and I have also to take into account compliance with EMC.

What do you consider it's the best option?

Thank you so much. Best Regards.

Outcomes