AnsweredAssumed Answered

HMC439QS16Q : Error Voltage

Question asked by AkiraO on Sep 27, 2015
Latest reply on Oct 1, 2015 by MRichardson

Hello

 

How much can we get the error voltage at following conditions?

REF input (3pin) : 1000MHz CW

VCO input (6pin) : 1000MHz plus (10us)

In this case, can we get 0Vdc under the phase differemce is 0 rad, -0.4Vdc under the phase differemce is -p/2 rad and +0.4Vdc under the phase differemce is p/2 rad as the error voltage in the term of 10us plus?

 

Besr Regards,

Akira

Outcomes