AnsweredAssumed Answered

Versions of the AD-FMCMOTCON2-EBZ motor boards

Question asked by valverj on Sep 25, 2015
Latest reply on Oct 6, 2015 by valverj

Hello,

 

I have the zedboard plus the AD-FMCMOTCON2-EBZ and a model for the control of the motor in Matlab for the AD-FMCMOTCON1-EBZ - Controller board.

 

If I want to reuse that model, do I need to update the reference design or/and the Linux Image? are there changes in the pins or controller connections? I am trying to make it work, and although the model is connecting to the board, I cannot make the motor spin while it is working on the other board.

 

Thanks a lot in advance

Outcomes